Settings Instructions
The Settings Instructions change the value of the drive's resource.
SET Instruction
The SET instruction sets a destination parameter (user variable, drive object or digital output) equal to the source parameter. It is also possible to set or reset a single bit. Read-only drive objects cannot be chosen as destination parameter.
When setting a digital output, the values other than 0 (1, 2, 3, etc.) are considered equal to logic = '1'( output closed).